AXIS#.VL.KP

Description

AXIS#.VL.KP sets the proportional gain of the velocity loop.

The idealized velocity loop bandwidth in Hz is:

Rotary motor:

Bandwidth (Hz) = AXIS#.VL.KP *Kt/ (2π *Jm)

Where:

Kt= motor torque constant, in units of Nm/Arms

Jm = motor inertia, in units of kg*m²

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

A/(rad/sec)

Range

0 to 2,147,483.008

Default Value

0

Data Type

Float
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
AXIS1.VL.KP

5011h

01h

Signed32

-

1000:1

Read/Write

No

AXIS2.VL.KP

5111h

01h

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.VL.KP

6029

178D

Signed32

Read/Write

-

AXIS2.VL.KP

71565

1178

Signed32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.VL.KP

6029

Float

Read/Write

-